NXObjectAttributeType Enumeration¶
NXOpen.NXObject.AttributeType is an alias for NXOpen.NXObjectAttributeType
-
class
NXOpen.
NXObjectAttributeType
¶ Bases:
object
Specifies attribute type.
NOTE: Attributes of type reference are also string attributes. The reference type as such is deprecated.
Enum Members
Enum Member Enum Member Description Invalid InvalidNull NullBoolean BooleanInteger IntegerReal RealString StringTime Time and DateReference Deprecated. Do not use in new code. Previously used to denote string attributes holding a ReferenceValueAny All types (used only for queries)-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-