PlaneTypesAlternateType Enumeration¶
NXOpen.PlaneTypes.AlternateType is an alias for NXOpen.PlaneTypesAlternateType
-
class
NXOpen.
PlaneTypesAlternateType
¶ Bases:
object
Represents the alternate solutions.
The system can have up to 4 alternate solutions depending upon the method. For example, if the user picks a point the system creates a plane through the point parallel to the XY plane. However, there are 2 additional solutions. The first is a plane through the point and the YZ plane. And the second is a plane through the point and XZ plane.
Enum Members
Enum Member Enum Member Description One First alternate solutionTwo Second alternate solutionThree Third alternate solutionFour Fourth alternate solutionFive Fifth alternate solutionSix Sixth alternate solution-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-