HumanPosturePredictionBuilderSteeringWheelPedalType Enumeration¶
NXOpen.HumanPosturePredictionBuilder.SteeringWheelPedalType is an alias for NXOpen.HumanPosturePredictionBuilderSteeringWheelPedalType
-
class
NXOpen.
HumanPosturePredictionBuilderSteeringWheelPedalType
¶ Bases:
object
This enum represents the steering wheel or pedal type, if there is no steering wheel or pedal, use csys as steering wheel and pedal type
Enum Members
the position and orientation of hand or foot “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-