ObjectSelector Class¶
-
class
NXOpen.
ObjectSelector
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.ObjectSelector
to be used when exporting the the selected objects from NX part.This class is created using
NXOpen.DexManager
. Creator not available in KF.New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
SelectionComp | Returns the selection comp. |
SelectionScope | Returns or sets the selection scope option. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ObjectSelectorScope Enumeration | Represents the selection scope |
Property Detail¶
SelectionComp¶
-
ObjectSelector.
SelectionComp
¶ Returns the selection comp.
This holds the list of selected objects.
-------------------------------------
Getter Method
Signature
SelectionComp()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX5.0.0.
License requirements: None.
SelectionScope¶
-
ObjectSelector.
SelectionScope
¶ Returns or sets the selection scope option.
This will decide if entire part should be exported or only some objects.
-------------------------------------
Getter Method
Signature
SelectionScope()
Returns: Return type: NXOpen.ObjectSelectorScope
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectionScope(selectionScope)
Parameters: selectionScope ( NXOpen.ObjectSelectorScope
) –New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ObjectSelector.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.