PlaneTypesFrenetSubtype Enumeration¶
NXOpen.PlaneTypes.FrenetSubtype is an alias for NXOpen.PlaneTypesFrenetSubtype
-
class
NXOpen.
PlaneTypesFrenetSubtype
¶ Bases:
object
Specify the subtypes for on_curve type of plane, where alternate solution is not enough to handle the situation after enhancement to this specific plane type.
Considering legacy data, these subtypes must match those already defined in the file “datum.h”
Enum Members
Enum Member Enum Member Description NotSpecified Subtype is not specifiedTangent Tangent to path, = FRENET_TANGENTNormal Normal to path, = FRENET_NORMALBinormal Binormal to path, = FRENET_BINORMALProject Reference to an object, = FRENET_PROJECTThruPoint Thru point type and normal to pathNormalToVector Normal to a vectorParallelToVector Parallel to a vectorThruAxis Thru axis typeThruPointNormalToVector Thru point and normal to a vectorThruPointParallelToVector Thru point and parallel to a vectorThruPointThruAxis Thru point and thru axis typeThruPointNormal Thru point and tangent_to_pathThruPointBinormal Thru point and binormal to pathThruPointProject Thru point and relative to object-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-