SelectionSelectionType Enumeration¶
NXOpen.Selection.SelectionType is an alias for NXOpen.SelectionSelectionType
-
class
NXOpen.
SelectionSelectionType
¶ Bases:
object
Indicates the general class of object to filter selection.
Enum Members
Enum Member Enum Member Description All Filter to select all object typesFeatures Filter to select all feature typesCurves Filter to select all curve typesFaces Filter to select all face typesEdges Filter to select all edge typesCurvesAndEdges Filter to select all curve and edge types-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-