WidthDefinition Class¶
-
class
NXOpen.
WidthDefinition
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.WidthDefinition
, which is a representation of an NX width palette.It gives the units in which all the widths are stored, single width information, the 3 custom width definitions, and an entry for each color.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Single | Returns or sets the single width type selection |
SingleSource | Returns or sets the single source. |
SingleWidth | Returns or sets the single width. |
Tag | Returns the Tag for this object. |
Units | Returns or sets the units. |
Use | Returns or sets the ‘use’ member. |
Methods¶
Method | Description |
---|---|
GetColorWidths | Gets the color widths. |
GetCustomWidths | Gets the custom widths array. |
Property Detail¶
Single¶
-
WidthDefinition.
Single
¶ Returns or sets the single width type selection
-------------------------------------
Getter Method
Signature
Single()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Single(single)
Parameters: single (int) – New in version NX5.0.0.
License requirements: None.
SingleSource¶
-
WidthDefinition.
SingleSource
¶ Returns or sets the single source.
The ‘single_source’ member contains a value when the ‘single’ member is CGME_width_std or CGME_width_custom. The value is the index in the ‘custom’ width array or the standard width index value. Both are assumed to be in internal order, normal, thick, and thin for 0, 1, and 2, respectively.
-------------------------------------
Getter Method
Signature
SingleSource()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SingleSource(singleSource)
Parameters: singleSource (int) – New in version NX5.0.0.
License requirements: None.
SingleWidth¶
-
WidthDefinition.
SingleWidth
¶ Returns or sets the single width.
The ‘single_width’ member contains the last-typed value for the user-defined width to use when CGME_width_user is selected for member ‘single’.
-------------------------------------
Getter Method
Signature
SingleWidth()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SingleWidth(singleWidth)
Parameters: singleWidth (float) – New in version NX5.0.0.
License requirements: None.
Units¶
-
WidthDefinition.
Units
¶ Returns or sets the units.
All the widths are stored in these units.
-------------------------------------
Getter Method
Signature
Units()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Units(units)
Parameters: units (int) – New in version NX5.0.0.
License requirements: None.
Use¶
-
WidthDefinition.
Use
¶ Returns or sets the ‘use’ member.
The use member specifies the primary selection of which type of width assignment to use.
-------------------------------------
Getter Method
Signature
Use()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Use(use)
Parameters: use (int) – New in version NX5.0.0.
License requirements: None.
Method Detail¶
GetColorWidths¶
-
WidthDefinition.
GetColorWidths
¶ Gets the color widths.
The ‘widths’ array is indexed by the color index straight out of the database, or 1-216. Therefore the array is one longer than the actual number of colors, or 217.
Signature
GetColorWidths()
Returns: Array of ColorWidth objects. Return type: list of NXOpen.ColorWidth
New in version NX5.0.0.
License requirements: None.
GetCustomWidths¶
-
WidthDefinition.
GetCustomWidths
¶ Gets the custom widths array.
There will be 3 CustomWidth objects.
Signature
GetCustomWidths()
Returns: Array of CustomWidth objects. Return type: list of NXOpen.CustomWidth
New in version NX5.0.0.
License requirements: None.