UpdateFailureOption Enumeration¶
NXOpen.Update.FailureOption is an alias for NXOpen.UpdateFailureOption
-
class
NXOpen.
UpdateFailureOption
¶ Bases:
object
Specifies the action to take when an object fails to update.
New in version NX7.5.0.
Enum Members
Enum Member Enum Member Description NoOption No optionUndo Perform undoSuppress Suppress failing objectSuppressAll Suppress failing objects and subsequent objectsAccept Accept failure of failing objectsAcceptAll Accept failure of failing objects and subsequent objectsDelete Delete failing objectDeleteDependents Delete failing object and its dependentsInterrupt Interrupt update upon failure-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-