OffsetCollection Class¶
-
class
NXOpen.
OffsetCollection
¶ Bases:
object
Represents a collection of
NXOpen.Offset
.Iterating this collection only returns live uncondemned objects contained in the owning part of the collection. Note that
NXOpen.Offset
is a smart object and many smart objects are condemned as they only exist to support other objects and are not displayed. Condemned objects will be deleted when their references go away. To obtain an instance of this class, refer toNXOpen.BasePart
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
CreateCurvature | Creates a NXOpen.Offset on a NXOpen.ICurve using a NXOpen.Scalar representing the t parameter. |
CreateCurvatureDerivative | Creates a NXOpen.Offset on a NXOpen.ICurve using a NXOpen.Scalar representing the t parameter. |
CreateOffset | Create an NXOpen.Offset without parameters. |
CreateOffsetCylindrical | Creates a smart cylindrical NXOpen.Offset . |
CreateOffsetRectangular | Create an NXOpen.Offset using X, Y and Z deltas. |
CreateOffsetSpherical | Creates a smart spherical NXOpen.Offset . |
Method Detail¶
CreateCurvature¶
-
OffsetCollection.
CreateCurvature
¶ Overloaded method CreateCurvature
CreateCurvature(icurve, t, updateOption)
CreateCurvature(atPoint, icurve, updateOption)
CreateCurvature(face, u, v, absoluteUv, option, sectionDirection, updateOption)
CreateCurvature(atPoint, face, option, sectionDirection, updateOption)
CreateCurvature(face, u, v, absoluteUv, sectionAngle, updateOption)
-------------------------------------
Creates a
NXOpen.Offset
on aNXOpen.ICurve
using aNXOpen.Scalar
representing the t parameter. The Offset created represents curvature of the curve at parameter t.Signature
CreateCurvature(icurve, t, updateOption)
Parameters: - icurve (
NXOpen.ICurve
) –NXOpen.Curve
orNXOpen.Edge
- t (
NXOpen.Scalar
) – - updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
Creates a
NXOpen.Offset
on aNXOpen.ICurve
using aNXOpen.Point
. The Offset created represents curvature of the curve at a point. The input point could be an extract point whose parent point is a point on curve. User can optionally supply a curve in which case it is honored instead of looking for the parent curve of the input point. In that case input point is projected on the curve to find the curvature at the projected location.Signature
CreateCurvature(atPoint, icurve, updateOption)
Parameters: - atPoint (
NXOpen.Point
) – An extract point or a non associative point in which case a curve should be specified. - icurve (
NXOpen.ICurve
) – OptionalNXOpen.Curve
orNXOpen.Edge
input - updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
Creates a
NXOpen.Offset
on aNXOpen.Face
using two :py:class:`NXOpen.Scalar`s representing the u and v parameters with option of direction on the face. The Offset created represents the curvature of the face at u and v parameter in a direction specified by the option.Signature
CreateCurvature(face, u, v, absoluteUv, option, sectionDirection, updateOption)
Parameters: - face (
NXOpen.Face
) – - u (
NXOpen.Scalar
) – - v (
NXOpen.Scalar
) – - absoluteUv (bool) – true if u and v are absolute parameters
- option (
NXOpen.OffsetOnFaceOption
) – - sectionDirection (
NXOpen.Direction
) – necessary when option isNXOpen.OffsetOnFaceOption.Section
- updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
Creates a
NXOpen.Offset
on aNXOpen.Face
using aNXOpen.Point
. The Offset created represents the curvature of the face at a point in a direction specified by the option. The input point could be a point on curve whose parent curve is an edge or a curve on surface feature. Or it could be an extract point whose parent point is a point on face. User can optionally supply a face in which case it is honored instead of looking for the parent face of the input point. In that case input point is projected on the face to find the curvature at the projected location.Signature
CreateCurvature(atPoint, face, option, sectionDirection, updateOption)
Parameters: - atPoint (
NXOpen.Point
) – A point on curve or an extract point. In case of a non associative point a face must be specified. - face (
NXOpen.Face
) – Optional input - option (
NXOpen.OffsetOnFaceOption
) – - sectionDirection (
NXOpen.SmartObject
) – An object of typeNXOpen.Direction
orNXOpen.Scalar
and is necessary when option isNXOpen.OffsetOnFaceOption.Section
- updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
Creates a sectional
NXOpen.Offset
on aNXOpen.Face
using twoNXOpen.Scalar`s representing the u and v parameters and a :py:class:`NXOpen.Scalar
representing section angle measured with respect to positive U parameter direction at u and v parameters of the face. The Offset created represents the curvature of the face at u and v parameter in the sectional direction.Signature
CreateCurvature(face, u, v, absoluteUv, sectionAngle, updateOption)
Parameters: - face (
NXOpen.Face
) – - u (
NXOpen.Scalar
) – - v (
NXOpen.Scalar
) – - absoluteUv (bool) – true if u and v are absolute parameters
- sectionAngle (
NXOpen.Scalar
) – measured in degree - updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
CreateCurvatureDerivative¶
-
OffsetCollection.
CreateCurvatureDerivative
¶ Overloaded method CreateCurvatureDerivative
CreateCurvatureDerivative(icurve, t, updateOption)
CreateCurvatureDerivative(atPoint, icurve, updateOption)
CreateCurvatureDerivative(face, u, v, absoluteUv, option, sectionDirection, updateOption)
CreateCurvatureDerivative(atPoint, face, option, sectionDirection, updateOption)
CreateCurvatureDerivative(face, u, v, absoluteUv, sectionAngle, updateOption)
-------------------------------------
Creates a
NXOpen.Offset
on aNXOpen.ICurve
using aNXOpen.Scalar
representing the t parameter. The Offset created represents curvature derivative of the curve at parameter t.Signature
CreateCurvatureDerivative(icurve, t, updateOption)
Parameters: - icurve (
NXOpen.ICurve
) –NXOpen.Curve
orNXOpen.Edge
- t (
NXOpen.Scalar
) – - updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
Creates a
NXOpen.Offset
on aNXOpen.ICurve
using aNXOpen.Point
. The Offset created represents curvature derivative of the curve at a point. The input point could be an extract point whose parent point is a point on curve. User can optionally supply a curve in which case it is honored instead of looking for the parent curve of the input point. In that case input point is projected on the curve to find the curvature derivative at the projected location.Signature
CreateCurvatureDerivative(atPoint, icurve, updateOption)
Parameters: - atPoint (
NXOpen.Point
) – An extract point or a non associative point in which case a curve should be specified. - icurve (
NXOpen.ICurve
) – OptionalNXOpen.Curve
orNXOpen.Edge
input - updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
Creates a
NXOpen.Offset
on aNXOpen.Face
using two :py:class:`NXOpen.Scalar`s representing the u and v parameters with option of direction on the face. The Offset created represents the curvature derivative of the face at u and v parameter in a direction specified by the option.Signature
CreateCurvatureDerivative(face, u, v, absoluteUv, option, sectionDirection, updateOption)
Parameters: - face (
NXOpen.Face
) – - u (
NXOpen.Scalar
) – - v (
NXOpen.Scalar
) – - absoluteUv (bool) – true if u and v are absolute parameters
- option (
NXOpen.OffsetOnFaceOption
) – - sectionDirection (
NXOpen.Direction
) – necessary when option isNXOpen.OffsetOnFaceOption.Section
- updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
Creates a
NXOpen.Offset
on aNXOpen.Face
using aNXOpen.Point
. The Offset created represents the curvature derivative of the face at a point in a direction specified by the option. The input point could be a point on curve whose parent curve is an edge or a curve on surface feature. Or it could be an extract point whose parent point is a point on face. User can optionally supply a face in which case it is honored instead of looking for the parent face of the input point. In that case input point is projected on the face to find the curvature derivative at the projected location.Signature
CreateCurvatureDerivative(atPoint, face, option, sectionDirection, updateOption)
Parameters: - atPoint (
NXOpen.Point
) – A point on curve or an extract point. In case of a non associative point a face must be specified. - face (
NXOpen.Face
) – Optional input - option (
NXOpen.OffsetOnFaceOption
) – - sectionDirection (
NXOpen.SmartObject
) – An object of typeNXOpen.Direction
orNXOpen.Scalar
and is necessary when option isNXOpen.OffsetOnFaceOption.Section
- updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
Creates a sectional
NXOpen.Offset
on aNXOpen.Face
using twoNXOpen.Scalar`s representing the u and v parameters and a :py:class:`NXOpen.Scalar
representing section angle measured with respect to positive U parameter direction at u and v parameters of the face. The Offset created represents the curvature derivative of the face at u and v parameter in the sectional direction.Signature
CreateCurvatureDerivative(face, u, v, absoluteUv, sectionAngle, updateOption)
Parameters: - face (
NXOpen.Face
) – - u (
NXOpen.Scalar
) – - v (
NXOpen.Scalar
) – - absoluteUv (bool) – true if u and v are absolute parameters
- sectionAngle (
NXOpen.Scalar
) – measured in degree - updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
CreateOffset¶
-
OffsetCollection.
CreateOffset
¶ Overloaded method CreateOffset
CreateOffset(origin, vector, updateOption)
CreateOffset(direction, distance, updateOption)
CreateOffset(offsetIn, xform, updateOption)
-------------------------------------
Create an
NXOpen.Offset
without parameters.Signature
CreateOffset(origin, vector, updateOption)
Parameters: - origin (
NXOpen.Point3d
) – Point of Offset - vector (
NXOpen.Vector3d
) – Offset vector - updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
Creates an
NXOpen.Offset
using a SmartNXOpen.Direction
and distance.Signature
CreateOffset(direction, distance, updateOption)
Parameters: - direction (
NXOpen.Direction
) – - distance (
NXOpen.Scalar
) – Distance along direction - updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
Creates a
NXOpen.Offset
via an extractNXOpen.Offset
with optional transformation.Signature
CreateOffset(offsetIn, xform, updateOption)
Parameters: - offsetIn (
NXOpen.Offset
) – Offset extract - xform (
NXOpen.Xform
) – Optional transformation - updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
CreateOffsetCylindrical¶
-
OffsetCollection.
CreateOffsetCylindrical
¶ Creates a smart cylindrical
NXOpen.Offset
.The radius, angle, and zdelta are the three parameters of cylindrical coordinates.
Signature
CreateOffsetCylindrical(radius, angle, deltaZ, updateOption)
Parameters: - radius (
NXOpen.Scalar
) – - angle (
NXOpen.Scalar
) – Angle in radians - deltaZ (
NXOpen.Scalar
) – Delta along axis of cylinder - updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
- radius (
CreateOffsetRectangular¶
-
OffsetCollection.
CreateOffsetRectangular
¶ Create an
NXOpen.Offset
using X, Y and Z deltas.Signature
CreateOffsetRectangular(deltaX, deltaY, deltaZ, updateOption)
Parameters: - deltaX (
NXOpen.Scalar
) – - deltaY (
NXOpen.Scalar
) – - deltaZ (
NXOpen.Scalar
) – - updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
- deltaX (
CreateOffsetSpherical¶
-
OffsetCollection.
CreateOffsetSpherical
¶ Creates a smart spherical
NXOpen.Offset
.The radius, angle1, and angle2 are the three parameters of spherical coordinates.
Signature
CreateOffsetSpherical(radius, angle1, angle2, updateOption)
Parameters: - radius (
NXOpen.Scalar
) – - angle1 (
NXOpen.Scalar
) – Longitude angle in radians - angle2 (
NXOpen.Scalar
) – Colatitude angle in radians - updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
- radius (