OffsetOnFaceOption Enumeration¶
NXOpen.Offset.OnFaceOption is an alias for NXOpen.OffsetOnFaceOption
-
class
NXOpen.
OffsetOnFaceOption
¶ Bases:
object
Specifies the offset direction in relation to a face.
Enum Members
Enum Member Enum Member Description U Creates offset representing curvature in U parameter direction on face.V Creates offset representing curvature in V parameter direction on face.Section Creates offset representing curvature in a sectional direction on face.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-