AxisTypes Enumeration¶
NXOpen.Axis.Types is an alias for NXOpen.AxisTypes
-
class
NXOpen.
AxisTypes
¶ Bases:
object
Defines types of axes based on their associativity
Enum Members
Enum Member Enum Member Description NonAssociative non-associativePointAndDirection the axis is defined by aNXOpen.Point
andNXOpen.CAE.Xyplot.AxisDirection
Other the type is not one of the other enumerated types-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-