AxisDirection Enumeration

class NXOpen.CAE.Xyplot.AxisDirection

Bases: object

Represents the axis direction Enum Members

Enum Member Enum Member Description
X
X-axis
Y
Y-axis
Z
Z-axis
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.