SketchDimensionOption Enumeration¶
NXOpen.Sketch.DimensionOption is an alias for NXOpen.SketchDimensionOption
-
class
NXOpen.
SketchDimensionOption
¶ Bases:
object
Used by
NXOpen.Sketch.CreateDimension()
,NXOpen.Sketch.CreateRadialDimension()
NXOpen.Sketch.CreateDiameterDimension()
andNXOpen.Sketch.CreatePerimeterDimension()
to determine whether to create driving or reference dimensionEnum Members
.
- . csv-table::
header: “Enum Member”, “Enum Member Description” “CreateAsDriving”, ” Create dimension as driving ” “CreateAsReference”, ” Create dimension as reference ” “CreateAsAutomatic”, ” Create dimension as automatic “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.