ErrorList Class¶
-
class
NXOpen.
ErrorList
¶ Bases:
NXOpen.TransientObject
Represents a list of errors
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
Clear | Clears the list |
Dispose | Frees the object from memory. |
GetErrorInfo | Gets the nth error information structure in the list @return the nth error information structure in the list |
Property Detail¶
Method Detail¶
Clear¶
-
ErrorList.
Clear
¶ Clears the list
Signature
Clear()
New in version NX3.0.0.
License requirements: None.
Dispose¶
-
ErrorList.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.
GetErrorInfo¶
-
ErrorList.
GetErrorInfo
¶ Gets the nth error information structure in the list
Signature
GetErrorInfo(n)
Parameters: n (int) – must be between 0 and (length of the list - 1) Returns: the nth error information structure in the list Return type: NXOpen.ErrorInfo
New in version NX3.0.0.
License requirements: None.