RuleManagerFilter Enumeration¶
NXOpen.RuleManager.Filter is an alias for NXOpen.RuleManagerFilter
-
class
NXOpen.
RuleManagerFilter
¶ Bases:
object
The filter option for asking for classes.
Enum Members
Enum Member Enum Member Description User User classes onlySystem System classes onlyBoth Both user and system classesUserPlus User and application classesUserLoaded User classes that are loadedSystemLoaded System classes that are loadedBothLoaded System and user classes that are loadedUserPlusLoaded User and application classes that are loaded-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-