PlaneCollection Class¶
-
class
NXOpen.
PlaneCollection
¶ Bases:
object
Represents a collection of
NXOpen.Plane
.Iterating this collection only returns live uncondemned objects contained in the owning part of the collection. Note that
NXOpen.Plane
is a smart object and many smart objects are condemned as they only exist to support other objects and are not displayed. Condemned objects will be deleted when their references go away. To obtain an instance of this class, refer toNXOpen.BasePart
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateFixedPlane | Creates a Plane without parameters. |
CreatePlane | Creates a Plane without parameters. |
Method Detail¶
CreateFixedPlane¶
-
PlaneCollection.
CreateFixedPlane
¶ Overloaded method CreateFixedPlane
CreateFixedPlane(origin, matrix)
CreateFixedPlane(origin, matrix, show)
-------------------------------------
Creates a
Plane
without parameters.Signature
CreateFixedPlane(origin, matrix)
Parameters: - origin (
NXOpen.Point3d
) – Plane Origin - matrix (
NXOpen.Matrix3x3
) – Plane Matrix
Returns: the plane
Return type: New in version NX11.0.0.
License requirements: None.
-------------------------------------
Creates a
Plane
without parameters. Has an additional input flag to control if the plane is visible or not after creation.Signature
CreateFixedPlane(origin, matrix, show)
Parameters: - origin (
NXOpen.Point3d
) – Plane Origin - matrix (
NXOpen.Matrix3x3
) – Plane Matrix - show (bool) – Control whether to show the plane object
Returns: the plane
Return type: New in version NX11.0.0.
License requirements: None.
-------------------------------------
CreatePlane¶
-
PlaneCollection.
CreatePlane
¶ Overloaded method CreatePlane
CreatePlane(origin, normal, updateOption)
CreatePlane(datum)
CreatePlane(method, alternate, origin, normal, expression, flip, percent, geometry)
-------------------------------------
Creates a
Plane
without parameters.Signature
CreatePlane(origin, normal, updateOption)
Parameters: - origin (
NXOpen.Point3d
) – Plane Origin - normal (
NXOpen.Vector3d
) – Plane normal - updateOption (
NXOpen.SmartObjectUpdateOption
) – Smart Object update option
Returns: the plane
Return type: New in version NX4.0.0.
License requirements: None.
-------------------------------------
Creates a
Plane
using a datum plane feature.Signature
CreatePlane(datum)
Parameters: datum ( NXOpen.Features.Feature
) – Datum FeatureReturns: the plane Return type: NXOpen.Plane
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Creates a
Plane
using a datum plane feature.Signature
CreatePlane(method, alternate, origin, normal, expression, flip, percent, geometry)
Parameters: - method (
NXOpen.PlaneTypesMethodType
) – - alternate (
NXOpen.PlaneTypesAlternateType
) – - origin (
NXOpen.Point3d
) – Plane Origin - normal (
NXOpen.Vector3d
) – Plane normal - expression (str) – offset value
- flip (bool) – flip direction
- percent (bool) – arclength or percent value
- geometry (list of
NXOpen.NXObject
) –
Returns: the plane
Return type: New in version NX4.0.0.
License requirements: None.
-------------------------------------