PlaneTypesMethodType Enumeration¶
NXOpen.PlaneTypes.MethodType is an alias for NXOpen.PlaneTypesMethodType
-
class
NXOpen.
PlaneTypesMethodType
¶ Bases:
object
Specifies different method types of selected geometries
Enum Members
Enum Member Enum Member Description Undefined Not definedInferred Inferred methodCoincident Plane of object methodCoincidentFaceAxis Though face axis methodCoincidentPerpLinear Through linear perpendicluar to linear methodParallel Parallel methodParallelPoint Parallel to plane through point methodPerpendicular Perpendicular to plane methodPerpendicularPoint Perpendicular to plane though point methodPerpendicularLinear Perpendicular to plane through linear methodCenter Center methodTangent Tangent methodTangentFace Tangent to face methodTangentPoint Tangent to face through point methodTangentLinear Tangent to face through linear methodTangentParPlane Tangent to face parallel to plane methodTangentPerpPlane Tangent to face perpendicular to plane methodTangentTwoFaces Tangent to two faces methodTangentAnglePlane Tangent to a cyl face at an angle to a planar faceDistance Distance methodAngle Angle methodFrenet Frenet methodPointDir Point and direction methodPoint Point methodTwoPoints Two Points methodThreePoints Three points methodLine Line methodTwoLines Two line methodCurvePoint On curve through point methodFixedX Fixed plane perpendicular to X thru WCSFixedY Fixed plane perpendicular to Y thru WCSFixedZ Fixed plane perpendicular to Z thru WCSFixedXyCsys Fixed plane perpendicular to Z thru X-Y plane of CSYSCoefficients Fixed plane defined by coefficientsInferredTop Inferred Top methodTangentInfer Inferred Tangent methodPointInfer Inferred Point methodFaceAxisPoint Through Face Axis at PointFixed Fixed Method (super type including any non-associative, xy, yz, xz, and coefficientFixedView View Plane methodConstructed Constructed types: super type for At Angle Parallel/Perpendicular or Tangent Angle to Plane Parallel/Perpendicular-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-