LineWidthBuilder Class¶
-
class
NXOpen.
LineWidthBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.LineWidthBuilder
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
Width | Returns or sets the width. |
WidthOption | Returns or sets the width option |
Methods¶
Method | Description |
---|---|
IsValidOption | Determines if the specified width option is supported. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Width¶
-
LineWidthBuilder.
Width
¶ Returns or sets the width.
Used when the width option is set to
LineWidthOption.Assigned
.-------------------------------------
Getter Method
Signature
Width()
Returns: Return type: NXOpen.DisplayableObjectObjectWidth
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width(width)
Parameters: width ( NXOpen.DisplayableObjectObjectWidth
) –New in version NX8.5.0.
License requirements: None.
WidthOption¶
-
LineWidthBuilder.
WidthOption
¶ Returns or sets the width option
Use
NXOpen.LineWidthBuilder.IsValidOption()
to check whether the width option is supported by the builder.-------------------------------------
Getter Method
Signature
WidthOption()
Returns: Return type: NXOpen.LineWidthOption
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WidthOption(widthOption)
Parameters: widthOption ( NXOpen.LineWidthOption
) –New in version NX8.5.0.
License requirements: None.
Method Detail¶
IsValidOption¶
-
LineWidthBuilder.
IsValidOption
¶ Determines if the specified width option is supported.
Signature
IsValidOption(widthOption)
Parameters: widthOption ( NXOpen.LineWidthOption
) –Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
Validate¶
-
LineWidthBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.