PlotManager Class¶
-
class
NXOpen.
PlotManager
¶ Bases:
object
The PlotManager class provides methods to create Gateway Builder objects.
NXOpen.PrintBuilder
,NXOpen.PlotBuilder
,NXOpen.PrintPDFBuilder
, andNXOpen.CGMBuilder
are all created using theNXOpen.PlotManager
class. To obtain an instance of this class, refer toNXOpen.BasePart
New in version NX5.0.1.
Methods¶
Method | Description |
---|---|
CreateCgmBuilder | Create the CGMBuilder @return |
CreatePlotBuilder | Create the PlotBuilder @return |
CreatePrint3dBuilder | Create the Print3dBuilder @return |
CreatePrintBuilder | Create the PrintBuilder @return |
CreatePrintPdfbuilder | Create the PrintPDFBuilder @return |
Method Detail¶
CreateCgmBuilder¶
-
PlotManager.
CreateCgmBuilder
¶ Create the CGMBuilder
Signature
CreateCgmBuilder()
Returns: Return type: NXOpen.CGMBuilder
New in version NX6.0.0.
License requirements: None.
CreatePlotBuilder¶
-
PlotManager.
CreatePlotBuilder
¶ Create the PlotBuilder
Signature
CreatePlotBuilder()
Returns: Return type: NXOpen.PlotBuilder
New in version NX5.0.1.
License requirements: None.
CreatePrint3dBuilder¶
-
PlotManager.
CreatePrint3dBuilder
¶ Create the Print3dBuilder
Signature
CreatePrint3dBuilder()
Returns: Return type: NXOpen.Print3dBuilder
New in version NX11.0.0.
License requirements: None.
CreatePrintBuilder¶
-
PlotManager.
CreatePrintBuilder
¶ Create the PrintBuilder
Signature
CreatePrintBuilder()
Returns: Return type: NXOpen.PrintBuilder
New in version NX5.0.1.
License requirements: None.
CreatePrintPdfbuilder¶
-
PlotManager.
CreatePrintPdfbuilder
¶ Create the PrintPDFBuilder
Signature
CreatePrintPdfbuilder()
Returns: Return type: NXOpen.PrintPDFBuilder
New in version NX5.0.1.
License requirements: None.