SurfaceUVDirectionBuilder Class¶
-
class
NXOpen.
SurfaceUVDirectionBuilder
¶ Bases:
NXOpen.Builder
Represents an edit surface u/v direction builder that allows reversing or swapping parametric directions.
To create a new instance of this class, use
NXOpen.BodyCollection.CreateSurfaceUvdirectionBuilder()
Default values.
Property Value ReverseU 0 ReverseV 0 SwapUandV 0 New in version NX8.5.1.
Properties¶
Property | Description |
---|---|
ReverseU | Returns or sets the reverse u direction option. |
ReverseV | Returns or sets the reverse v direction option. |
SwapUandV | Returns or sets the swap u and v directions option. |
Tag | Returns the Tag for this object. |
TargetFace | Returns the target face; feature faces can not be operated on. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ReverseU¶
-
SurfaceUVDirectionBuilder.
ReverseU
¶ Returns or sets the reverse u direction option.
-------------------------------------
Getter Method
Signature
ReverseU()
Returns: Return type: bool New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseU(reverseU)
Parameters: reverseU (bool) – New in version NX8.5.1.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ReverseV¶
-
SurfaceUVDirectionBuilder.
ReverseV
¶ Returns or sets the reverse v direction option.
-------------------------------------
Getter Method
Signature
ReverseV()
Returns: Return type: bool New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseV(reverseV)
Parameters: reverseV (bool) – New in version NX8.5.1.
License requirements: studio_free_form (“STUDIO FREE FORM”)
SwapUandV¶
-
SurfaceUVDirectionBuilder.
SwapUandV
¶ Returns or sets the swap u and v directions option.
-------------------------------------
Getter Method
Signature
SwapUandV()
Returns: Return type: bool New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
SwapUandV(swapUandV)
Parameters: swapUandV (bool) – New in version NX8.5.1.
License requirements: studio_free_form (“STUDIO FREE FORM”)
TargetFace¶
-
SurfaceUVDirectionBuilder.
TargetFace
¶ Returns the target face; feature faces can not be operated on.
-------------------------------------
Getter Method
Signature
TargetFace()
Returns: Return type: NXOpen.SelectFaceList
New in version NX8.5.1.
License requirements: None.
Method Detail¶
Validate¶
-
SurfaceUVDirectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.