FaceAllBlendRule Class¶
-
class
NXOpen.
FaceAllBlendRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects all blend faces.New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the All Blend Faces rule: NXOpen.FaceAllBlendRule @return Body which creates this rule |
GetDefiningData | Gets the data for the All Blend Faces rule: NXOpen.FaceAllBlendRule |
Method Detail¶
Dispose¶
-
FaceAllBlendRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX5.0.0.
License requirements: None.
GetData¶
-
FaceAllBlendRule.
GetData
¶ Gets the data for the All Blend Faces rule:
NXOpen.FaceAllBlendRule
Signature
GetData()
Returns: Body which creates this rule Return type: NXOpen.Body
New in version NX5.0.0.
License requirements: None.
GetDefiningData¶
-
FaceAllBlendRule.
GetDefiningData
¶ Gets the data for the All Blend Faces rule:
NXOpen.FaceAllBlendRule
Signature
GetDefiningData()
Returns: a tuple Return type: A tuple consisting of (body, feature). body is a
NXOpen.Body
. Body which creates this rulefeature is aNXOpen.Features.Feature
. Feature which creates this rule .. versionadded:: NX8.5.0License requirements: None.