SketchAlternateSolutionOption Enumeration¶
NXOpen.Sketch.AlternateSolutionOption is an alias for NXOpen.SketchAlternateSolutionOption
-
class
NXOpen.
SketchAlternateSolutionOption
¶ Bases:
object
Indicates whether the alternate solution should be used instead of the regular solution.
The alternate solution for an arc is the portion of the full circle that is left out of the regular solution. For example, if the regular solution is an arc that goes from 0 to 45 degrees, the alternate solution will be an arc with the same center and origin but that goes from 45 degrees to 360.
Enum Members
Enum Member Enum Member Description False Use the regular solutionTrue Use the alternate solution-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-