FaceMergedRibFacesRule Class¶
-
class
NXOpen.
FaceMergedRibFacesRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects all merged rib faces.New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the rib faces rule: NXOpen.FaceMergedRibFacesRule |
GetDefiningData | Gets the data for the rib faces rule: NXOpen.FaceMergedRibFacesRule @return Faces which creates this rule |
GetSeedAndPointData | Gets the data for the rib faces rule: NXOpen.FaceMergedRibFacesRule |
Method Detail¶
Dispose¶
-
FaceMergedRibFacesRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX6.0.0.
License requirements: None.
GetData¶
-
FaceMergedRibFacesRule.
GetData
¶ Gets the data for the rib faces rule:
NXOpen.FaceMergedRibFacesRule
Signature
GetData()
Returns: a tuple Return type: A tuple consisting of (face, edge). face is a
NXOpen.Face
. Faces which creates this ruleedge is aNXOpen.Edge
. Edge which creates this rule .. versionadded:: NX6.0.0License requirements: gateway (“UG GATEWAY”)
GetDefiningData¶
-
FaceMergedRibFacesRule.
GetDefiningData
¶ Gets the data for the rib faces rule:
NXOpen.FaceMergedRibFacesRule
Signature
GetDefiningData()
Returns: a tuple Return type: A tuple consisting of (face, edge, includeBoundaryBlends). face is a
NXOpen.Face
. Faces which creates this ruleedge is aNXOpen.Edge
. Edge which creates this ruleincludeBoundaryBlends is a bool. true if the rule is to identify any blends at the boundary .. versionadded:: NX6.0.0License requirements: gateway (“UG GATEWAY”)
GetSeedAndPointData¶
-
FaceMergedRibFacesRule.
GetSeedAndPointData
¶ Gets the data for the rib faces rule:
NXOpen.FaceMergedRibFacesRule
Signature
GetSeedAndPointData()
Returns: a tuple Return type: A tuple consisting of (face, seedPt). face is a
NXOpen.Face
. Faces which creates this ruleseedPt is aNXOpen.Point3d
. Seed pick point point. .. versionadded:: NX8.0.0License requirements: gateway (“UG GATEWAY”)