LinkedPartManager Class¶
-
class
NXOpen.
LinkedPartManager
¶ Bases:
object
Represents the customization interface during linked mirror part creation and update.
The “map entity handler” customization callback is called during creation of linked mirror part and during update of the linked mirror part from source. One can provide a custom map between the candidate unmapped entities in the source part and candidate unmapped entities in the mirror part.
The “attribute edit handler” customization callback is called during creation of linked mirror part and during update of the linked mirror part from source. One can edit the attributes on entities in the mirror part using this callback.
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
AddAttributeEditHandler | Registers a user defined attribute edit method that is called whenever a linked mirror part is created or updated from source @return identifier of registered method (used to unregister the method) |
AddMapEntityHandler | Registers a user defined map entity method that is called whenever a linked mirror part is created or updated from source @return identifier of registered method (used to unregister the method) |
RemoveAttributeEditHandler | Unregisters the attribute edit handler |
RemoveMapEntityHandler | Unregisters the user defined map entity handler |
Method Detail¶
AddAttributeEditHandler¶
-
LinkedPartManager.
AddAttributeEditHandler
¶ Registers a user defined attribute edit method that is called whenever a linked mirror part is created or updated from source
Signature
AddAttributeEditHandler(handler)
Parameters: handler (CallableObject) – method to register Returns: identifier of registered method (used to unregister the method) Return type: int New in version NX8.5.0.
License requirements: None.
AddMapEntityHandler¶
-
LinkedPartManager.
AddMapEntityHandler
¶ Registers a user defined map entity method that is called whenever a linked mirror part is created or updated from source
Signature
AddMapEntityHandler(handler)
Parameters: handler (CallableObject) – method to register Returns: identifier of registered method (used to unregister the method) Return type: int New in version NX8.5.0.
License requirements: None.