CoordinateSystemCollection Class¶
-
class
NXOpen.
CoordinateSystemCollection
¶ Bases:
object
Represents a collection of
NXOpen.CoordinateSystem
.Iterating this collection only returns live uncondemned objects contained in the owning part of the collection. Note that
NXOpen.CoordinateSystem
is a smart object and many smart objects are condemned as they only exist to support other objects and are not displayed. Condemned objects will be deleted when their references go away. To obtain an instance of this class, refer toNXOpen.BasePart
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
CreateCoordinateSystem | Creates a new cartesian coordinate system @return The created CartesianCoordinateSystem |
CreateCylindricalCoordinateSystem | Creates a new cylindrical coordinate system @return The created CylindricalCoordinateSystem |
CreateSphericalCoordinateSystem | Creates a new spherical coordinate system @return The created SphericalCoordinateSystem |
Method Detail¶
CreateCoordinateSystem¶
-
CoordinateSystemCollection.
CreateCoordinateSystem
¶ Overloaded method CreateCoordinateSystem
CreateCoordinateSystem(origin, orientation, isTemporary)
CreateCoordinateSystem(origin, xDirection, yDirection)
CreateCoordinateSystem(origin, orientation, isTemporary)
CreateCoordinateSystem(xform, update)
-------------------------------------
Creates a new cartesian coordinate system
Signature
CreateCoordinateSystem(origin, orientation, isTemporary)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the new coordinate system (relative to the absolute coordinate system) - orientation (
NXOpen.Matrix3x3
) – Orientation of the new coordinate system (relative to the absolute coordinate system). Must be orthonormal. - isTemporary (bool) – If the coordinate system is temporary, it will not be displayed and it will not be saved in the part file
Returns: The created CartesianCoordinateSystem
Return type: New in version NX3.0.0.
License requirements: None.
-------------------------------------
Creates a new cartesian coordinate system
Signature
CreateCoordinateSystem(origin, xDirection, yDirection)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the new coordinate system (relative to the absolute coordinate system) - xDirection (
NXOpen.Vector3d
) – x direction of the new coordinate system (relative to the absolute coordinate system) - yDirection (
NXOpen.Vector3d
) – y direction of the new coordinate system (relative to the absolute coordinate system)
Returns: The created CartesianCoordinateSystem
Return type: New in version NX5.0.0.
License requirements: None.
-------------------------------------
Creates a new cartesian coordinate system
Signature
CreateCoordinateSystem(origin, orientation, isTemporary)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the new coordinate system (relative to the absolute coordinate system - orientation (
NXOpen.NXMatrix
) – Orientation of the new coordinate system - isTemporary (bool) – If the coordinate system is temporary, it will not be displayed and it will not be saved in the part file
Returns: The created CartesianCoordinateSystem
Return type: New in version NX3.0.0.
License requirements: None.
-------------------------------------
Creates a CartesianCoordinateSystem from a Xform and update option.
Signature
CreateCoordinateSystem(xform, update)
Parameters: - xform (
NXOpen.Xform
) – the Xform of the coordinate system - update (
NXOpen.SmartObjectUpdateOption
) – update option
Returns: The created CartesianCoordinateSystem
Return type: New in version NX4.0.0.
License requirements: None.
-------------------------------------
CreateCylindricalCoordinateSystem¶
-
CoordinateSystemCollection.
CreateCylindricalCoordinateSystem
¶ Overloaded method CreateCylindricalCoordinateSystem
CreateCylindricalCoordinateSystem(origin, xDirection, yDirection)
CreateCylindricalCoordinateSystem(origin, orientation, isTemporary)
CreateCylindricalCoordinateSystem(xform, update)
-------------------------------------
Creates a new cylindrical coordinate system
Signature
CreateCylindricalCoordinateSystem(origin, xDirection, yDirection)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the new coordinate system (relative to the absolute coordinate system) - xDirection (
NXOpen.Vector3d
) – x direction of the new coordinate system (relative to the absolute coordinate system) - yDirection (
NXOpen.Vector3d
) – y direction of the new coordinate system (relative to the absolute coordinate system)
Returns: The created CylindricalCoordinateSystem
Return type: New in version NX5.0.0.
License requirements: None.
-------------------------------------
Creates a new cylindrical coordinate system
Signature
CreateCylindricalCoordinateSystem(origin, orientation, isTemporary)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the new coordinate system (relative to the absolute coordinate system - orientation (
NXOpen.NXMatrix
) – Orientation of the new coordinate system - isTemporary (bool) – If the coordinate system is temporary, it will not be displayed and it will not be saved in the part file
Returns: The created CylindricalCoordinateSystem
Return type: New in version NX4.0.0.
License requirements: None.
-------------------------------------
Creates a CylindricalCoordinateSystem from a Xform and update option.
Signature
CreateCylindricalCoordinateSystem(xform, update)
Parameters: - xform (
NXOpen.Xform
) – the Xform of the coordinate system - update (
NXOpen.SmartObjectUpdateOption
) – update option
Returns: The created CylindricalCoordinateSystem
Return type: New in version NX4.0.0.
License requirements: None.
-------------------------------------
CreateSphericalCoordinateSystem¶
-
CoordinateSystemCollection.
CreateSphericalCoordinateSystem
¶ Overloaded method CreateSphericalCoordinateSystem
CreateSphericalCoordinateSystem(origin, xDirection, yDirection)
CreateSphericalCoordinateSystem(origin, orientation, isTemporary)
CreateSphericalCoordinateSystem(xform, update)
-------------------------------------
Creates a new spherical coordinate system
Signature
CreateSphericalCoordinateSystem(origin, xDirection, yDirection)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the new coordinate system (relative to the absolute coordinate system) - xDirection (
NXOpen.Vector3d
) – x direction of the new coordinate system (relative to the absolute coordinate system) - yDirection (
NXOpen.Vector3d
) – y direction of the new coordinate system (relative to the absolute coordinate system)
Returns: The created SphericalCoordinateSystem
Return type: New in version NX5.0.0.
License requirements: None.
-------------------------------------
Creates a new spherical coordinate system
Signature
CreateSphericalCoordinateSystem(origin, orientation, isTemporary)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the new coordinate system (relative to the absolute coordinate system - orientation (
NXOpen.NXMatrix
) – Orientation of the new coordinate system - isTemporary (bool) – If the coordinate system is temporary, it will not be displayed and it will not be saved in the part file
Returns: The created SphericalCoordinateSystem
Return type: New in version NX4.0.0.
License requirements: None.
-------------------------------------
Creates a SphericalCoordinateSystem from a Xform and update option.
Signature
CreateSphericalCoordinateSystem(xform, update)
Parameters: - xform (
NXOpen.Xform
) – the Xform of the coordinate system - update (
NXOpen.SmartObjectUpdateOption
) – update option
Returns: The created SphericalCoordinateSystem
Return type: New in version NX4.0.0.
License requirements: None.
-------------------------------------