EdgeMultipleSeedTangentRule Class¶
-
class
NXOpen.
EdgeMultipleSeedTangentRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects tangent connected edges from the body of the seed edge.This rule is different from
NXOpen.EdgeTangentRule
in that each collected edge can act as a seed. .. versionadded:: NX3.0.0
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the edge multiple seed tangent rule: NXOpen.EdgeMultipleSeedTangentRule |
Method Detail¶
Dispose¶
-
EdgeMultipleSeedTangentRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.
GetData¶
-
EdgeMultipleSeedTangentRule.
GetData
¶ Gets the data for the edge multiple seed tangent rule:
NXOpen.EdgeMultipleSeedTangentRule
Signature
GetData()
Returns: a tuple Return type: A tuple consisting of (seedEdges, angleTolerance, hasSameConvexity). seedEdges is a list of
NXOpen.Edge
. Seed edges angleTolerance is a float. Angle tolerance for tangent edges hasSameConvexity is a bool. True: will only find tangnet edges that has the same convexity .. versionadded:: NX3.0.0License requirements: gateway (“UG GATEWAY”)