LayoutDefinition Class¶
-
class
NXOpen.
LayoutDefinition
¶ Bases:
NXOpen.TransientObject
Represents the definition of a layout.
This includes the arrangement and location of the views in the arrangement.
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
Arrangement | Returns the arrangement type of the layout definition. |
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetView | Returns the NXOpen.View at specified position in layout. |
SetView | Sets the NXOpen.ModelingView at specified position in layout. |
Enumerations¶
LayoutDefinitionArrangementType Enumeration | Indicates the arrangement type of a layout. |
Property Detail¶
Arrangement¶
-
LayoutDefinition.
Arrangement
¶ Returns the arrangement type of the layout definition.
-------------------------------------
Getter Method
Signature
Arrangement()
Returns: Arrangement of layout :rtype:
NXOpen.LayoutDefinitionArrangementType
New in version NX3.0.0.
License requirements: None.
Method Detail¶
Dispose¶
-
LayoutDefinition.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.
GetView¶
-
LayoutDefinition.
GetView
¶ Returns the
NXOpen.View
at specified position in layout.The system throws an exception when a user enters an invalid position.
Signature
GetView(row, column)
Parameters: - row (int) – Row of view
- column (int) – Column of view
Returns: Return type: New in version NX3.0.0.
License requirements: None.
SetView¶
-
LayoutDefinition.
SetView
¶ Sets the
NXOpen.ModelingView
at specified position in layout.The system throws an exception when a user enters an invalid position
Signature
SetView(row, column, view)
Parameters: - row (int) – Row of view
- column (int) – Column of view
- view (
NXOpen.ModelingView
) –
New in version NX3.0.0.
License requirements: None.