PhysicalMaterialCollection Class¶
-
class
NXOpen.
PhysicalMaterialCollection
¶ Bases:
object
Represents the collection of all
NXOpen.PhysicalMaterial
objects in this PartTo obtain an instance of this class, refer to
NXOpen.MaterialManager
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
AnyBodiesWithoutMaterial | Returns true if there are bodies in the specified part that do not have a material assigned to them; false if all bodies in the part have a material assigned. |
AnyBodiesWithoutPreferredMaterial | Returns true if there are bodies that do not have the preferred material assigned to them and false if all bodies are assigned the preferred material. |
CopyMaterialFromLibrary | Creates an editable material (copy) in the part from a library material definition. |
CopyMaterialItemRevision | Creates an editable material (copy) in the part from a Teamcenter material item revision. |
CreateListBlockBuilder | Creates a NXOpen.PhysMat.PhysicalMaterialListBuilder that controls the physical materials list UI block look and feel as well as capturing the interactions so the values/settings can be journaled. |
CreateMaterialAssignBuilder | Creates a PhysMat. |
CreateMaterialLibmgrBuilder | Creates a PhysMat. |
CreatePhysicalMaterialBuilder | Creates a PhysMat. |
CreatePhysicalMaterialEditBuilder | Creates a PhysMat. |
CreatePhysicalMaterialInspectBuilder | Creates a PhysMat. |
DeleteMaterialsFromLibrary | Deletes the materials from a material library file. |
ExportMaterialsToLibrary | Writes out materials to a material library file. |
FindBodiesWithoutMaterial | Returns the bodies that don’t have a material assigned. |
FindBodiesWithoutPreferredMaterial | Returns the bodies that are not using the preferred material (either no material assigned or the non-preferred a different material assigned). |
FindObject | Finds the NXOpen.PhysicalMaterial with the given identifier as recorded in a journal. |
GetLoadedLibraryMaterial | Checks if a library material is loaded into a part file or not. |
GetLoadedMaterialItemRevision | Checks if a Teamcenter material item revision is loaded into a part file or not. |
GetUsedMaterials | Returns the materials used in the part @return Materials used |
InfoItemRevision | Displays the property values for the specified Teamcenter Material Item Revision in the information window. |
InfoItemRevisionToFile | Writes the property values for the specified Teamcenter Material Item Revision to a file. |
InfoLibraryMaterial | Displays the property values for the specified library material in the information window. |
InfoLibraryMaterialToFile | Writes the property values for the specified library material to a file. |
LoadFromLegacynxlibrary | Creates a non-editable material in the part from the legacy (phys_material. |
LoadFromLibrary | Creates a non-editable material in the part from a material library name. |
LoadFromMatmlLibrary | Creates a non-editable material in the part from a MatML file definition. |
LoadFromNxlibrary | Creates a non-editable material in the part from a NX Material Library definition. |
LoadFromNxmatmllibrary | Creates a non-editable material in the part from a NX MatML material definition. |
LoadMaterialItemRevision | Creates a non-editable material in the part from a Teamcenter material item revision. |
OutputMaterialsToLibrary | Writes out materials to a material library file. |
UpdateMaterialsInLibrary | Updates the materials in a material library file. |
Method Detail¶
AnyBodiesWithoutMaterial¶
-
PhysicalMaterialCollection.
AnyBodiesWithoutMaterial
¶ Returns true if there are bodies in the specified part that do not have a material assigned to them; false if all bodies in the part have a material assigned.
Signature
AnyBodiesWithoutMaterial()
Returns: Return type: bool New in version NX7.5.2.
License requirements: None.
AnyBodiesWithoutPreferredMaterial¶
-
PhysicalMaterialCollection.
AnyBodiesWithoutPreferredMaterial
¶ Returns true if there are bodies that do not have the preferred material assigned to them and false if all bodies are assigned the preferred material.
If there is not a preferred material specified, the return value is true.
Signature
AnyBodiesWithoutPreferredMaterial()
Returns: Return type: bool New in version NX7.5.3.
License requirements: None.
CopyMaterialFromLibrary¶
-
PhysicalMaterialCollection.
CopyMaterialFromLibrary
¶ Overloaded method CopyMaterialFromLibrary
CopyMaterialFromLibrary(libraryName, libraryReference)
CopyMaterialFromLibrary(libraryName, libraryReference, retainParentPedigree)
-------------------------------------
Creates an editable material (copy) in the part from a library material definition.
Signature
CopyMaterialFromLibrary(libraryName, libraryReference)
Parameters: - libraryName (str) – the fully qualified library name or if the leaf it will use the current directory, followed by the user and site directories set up in the customer defaults
- libraryReference (str) – the material name/identifier
Returns: the copied material
Return type: New in version NX6.0.4.
License requirements: None.
-------------------------------------
Creates an editable material (copy) in the part from a library material definition.
Signature
CopyMaterialFromLibrary(libraryName, libraryReference, retainParentPedigree)
Parameters: - libraryName (str) – the fully qualified library name or if the leaf it will use the current directory, followed by the user and site directories set up in the customer defaults
- libraryReference (str) – the material name/identifier
- retainParentPedigree (bool) – true indicates that the copied material should retain information about what library material it came from
Returns: the copied material
Return type: New in version NX8.5.0.
License requirements: None.
-------------------------------------
CopyMaterialItemRevision¶
-
PhysicalMaterialCollection.
CopyMaterialItemRevision
¶ Creates an editable material (copy) in the part from a Teamcenter material item revision.
Signature
CopyMaterialItemRevision(pcMatlItem, pcRevisionID)
Parameters: - pcMatlItem (str) – the material item
- pcRevisionID (str) – the revision identifier
Returns: the copied material
Return type: New in version NX7.5.3.
License requirements: None.
CreateListBlockBuilder¶
-
PhysicalMaterialCollection.
CreateListBlockBuilder
¶ Creates a
NXOpen.PhysMat.PhysicalMaterialListBuilder
that controls the physical materials list UI block look and feel as well as capturing the interactions so the values/settings can be journaled.Signature
CreateListBlockBuilder()
Returns: created NXOpen.PhysMat.PhysicalMaterialListBuilder
Return type: NXOpen.PhysMat.PhysicalMaterialListBuilder
New in version NX6.0.0.
License requirements: None.
CreateMaterialAssignBuilder¶
-
PhysicalMaterialCollection.
CreateMaterialAssignBuilder
¶ Creates a PhysMat.
MaterialAssignBuilder that is used to control/set the material assign UI as well as to assign materials to bodies.
Signature
CreateMaterialAssignBuilder()
Returns: created NXOpen.PhysMat.PhysicalMaterialAssignBuilder
Return type: NXOpen.PhysMat.PhysicalMaterialAssignBuilder
New in version NX6.0.0.
License requirements: None.
CreateMaterialLibmgrBuilder¶
-
PhysicalMaterialCollection.
CreateMaterialLibmgrBuilder
¶ Creates a PhysMat.
PhysicalMaterialLibMgrBuilder used by the material library manager UI to control the look and feel as well as capturing the interactions so the values/settings can be journaled.
Signature
CreateMaterialLibmgrBuilder()
Returns: created NXOpen.PhysMat.PhysicalMaterialLibMgrBuilder
Return type: NXOpen.PhysMat.PhysicalMaterialLibMgrBuilder
New in version NX6.0.2.
License requirements: None.
CreatePhysicalMaterialBuilder¶
-
PhysicalMaterialCollection.
CreatePhysicalMaterialBuilder
¶ Creates a PhysMat.
PhysicalMaterialBuilder used to create a physical materials of a given type
Signature
CreatePhysicalMaterialBuilder(materialType)
Parameters: materialType ( NXOpen.PhysicalMaterialType
) – Type ofNXOpen.PhysicalMaterial
to be createdReturns: created NXOpen.PhysicalMaterialBuilder
Return type: NXOpen.PhysicalMaterialBuilder
New in version NX6.0.0.
License requirements: None.
CreatePhysicalMaterialEditBuilder¶
-
PhysicalMaterialCollection.
CreatePhysicalMaterialEditBuilder
¶ Creates a PhysMat.
PhysicalMaterialBuilder used to edit physical materials.
Signature
CreatePhysicalMaterialEditBuilder(physicalMaterial)
Parameters: physicalMaterial ( NXOpen.PhysicalMaterial
) –NXOpen.PhysicalMaterial
to be editedReturns: created NXOpen.PhysicalMaterialBuilder
Return type: NXOpen.PhysicalMaterialBuilder
New in version NX6.0.0.
License requirements: None.
CreatePhysicalMaterialInspectBuilder¶
-
PhysicalMaterialCollection.
CreatePhysicalMaterialInspectBuilder
¶ Creates a PhysMat.
PhysicalMaterialBuilder used to inspect physical materials.
Signature
CreatePhysicalMaterialInspectBuilder(physicalMaterial)
Parameters: physicalMaterial ( NXOpen.PhysicalMaterial
) –NXOpen.PhysicalMaterial
to be inspectedReturns: created NXOpen.PhysicalMaterialBuilder
Return type: NXOpen.PhysicalMaterialBuilder
New in version NX7.5.0.
License requirements: None.
DeleteMaterialsFromLibrary¶
-
PhysicalMaterialCollection.
DeleteMaterialsFromLibrary
¶ Deletes the materials from a material library file.
Write access is needed for this operation.
Signature
DeleteMaterialsFromLibrary(pMatlNames, pcLibName)
Parameters: - pMatlNames (list of str) – Arrays of identifiers of the materials to be deleted from the library
- pcLibName (str) – Library to modify
New in version NX6.0.2.
License requirements: None.
ExportMaterialsToLibrary¶
-
PhysicalMaterialCollection.
ExportMaterialsToLibrary
¶ Writes out materials to a material library file.
These materials can be local material definitions or material definitions from other material libraries. The combination of the material name and library name identify a material definition. If the material definition is for a local material, the name is specified and the library name is specified as “”. Write access is needed for the Exported library. If the bUpdateLibraryReferences is set to true, the NX model is updated to reflect the exported library as the library the material is now referenced in.
Signature
ExportMaterialsToLibrary(pcMatlNames, pcLibNames, pcExportedLibName, bUpdateLibraryReference)
Parameters: - pcMatlNames (list of str) – Array of identifiers of the materials to be exported
- pcLibNames (list of str) – Array of library names corresponding to the material names
- pcExportedLibName (str) – The library to write the material definitions to
- bUpdateLibraryReference (bool) – true indicates that the library reference of loaded/local materials should now refer to the exported library, false indicates the library reference should remain unchanged
New in version NX7.5.2.
License requirements: None.
FindBodiesWithoutMaterial¶
-
PhysicalMaterialCollection.
FindBodiesWithoutMaterial
¶ Returns the bodies that don’t have a material assigned.
Signature
FindBodiesWithoutMaterial()
Returns: the array of bodies without a material Return type: list of NXOpen.TaggedObject
New in version NX7.5.2.
License requirements: None.
FindBodiesWithoutPreferredMaterial¶
-
PhysicalMaterialCollection.
FindBodiesWithoutPreferredMaterial
¶ Returns the bodies that are not using the preferred material (either no material assigned or the non-preferred a different material assigned).
Signature
FindBodiesWithoutPreferredMaterial()
Returns: the array of bodies not using preferred material Return type: list of NXOpen.TaggedObject
New in version NX7.5.2.
License requirements: None.
FindObject¶
-
PhysicalMaterialCollection.
FindObject
¶ Finds the
NXOpen.PhysicalMaterial
with the given identifier as recorded in a journal.An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: material found Return type: NXOpen.Material
New in version NX5.0.0.
License requirements: None.
GetLoadedLibraryMaterial¶
-
PhysicalMaterialCollection.
GetLoadedLibraryMaterial
¶ Checks if a library material is loaded into a part file or not.
If it is, the loaded material is returned.
Signature
GetLoadedLibraryMaterial(pcLibName, pcMatlName)
Parameters: - pcLibName (str) – the fully qualified library name or if the leaf it will use the current directory, followed by the user and site directories set up in the customer defaults
- pcMatlName (str) – the material name
Returns: the loaded material
Return type: New in version NX7.5.3.
License requirements: None.
GetLoadedMaterialItemRevision¶
-
PhysicalMaterialCollection.
GetLoadedMaterialItemRevision
¶ Checks if a Teamcenter material item revision is loaded into a part file or not.
If it is, the loaded material is returned.
Signature
GetLoadedMaterialItemRevision(pcMatlItem, pcRevisionID)
Parameters: - pcMatlItem (str) – the material item
- pcRevisionID (str) – the revision identifier
Returns: the loaded material
Return type: New in version NX7.5.3.
License requirements: None.
GetUsedMaterials¶
-
PhysicalMaterialCollection.
GetUsedMaterials
¶ Returns the materials used in the part
Signature
GetUsedMaterials()
Returns: Materials used Return type: list of NXOpen.PhysicalMaterial
New in version NX8.0.1.
License requirements: None.
InfoItemRevision¶
-
PhysicalMaterialCollection.
InfoItemRevision
¶ Displays the property values for the specified Teamcenter Material Item Revision in the information window.
Signature
InfoItemRevision(pcMaterialItem, pcRevision)
Parameters: - pcMaterialItem (str) – the material item
- pcRevision (str) – the revision identifier
New in version NX7.5.3.
License requirements: None.
InfoItemRevisionToFile¶
-
PhysicalMaterialCollection.
InfoItemRevisionToFile
¶ Writes the property values for the specified Teamcenter Material Item Revision to a file.
Signature
InfoItemRevisionToFile(pcMaterialItem, pcRevision, bOverride, pcFileName)
Parameters: - pcMaterialItem (str) – the material item
- pcRevision (str) – the revision identifier
- bOverride (bool) – if the file already exists, true override the file, false append to the file
- pcFileName (str) – the full path including filename of file where the information should be written
New in version NX7.5.3.
License requirements: None.
InfoLibraryMaterial¶
-
PhysicalMaterialCollection.
InfoLibraryMaterial
¶ Displays the property values for the specified library material in the information window.
Signature
InfoLibraryMaterial(pcLibAr, pcMatlNameAr)
Parameters: - pcLibAr (str) – the library name
- pcMatlNameAr (str) – the material name
New in version NX7.5.3.
License requirements: None.
InfoLibraryMaterialToFile¶
-
PhysicalMaterialCollection.
InfoLibraryMaterialToFile
¶ Writes the property values for the specified library material to a file.
Signature
InfoLibraryMaterialToFile(pcLibAr, pcMatlNameAr, bOverride, pcFileName)
Parameters: - pcLibAr (str) – the library name
- pcMatlNameAr (str) – the material name
- bOverride (bool) – if the file already exists, true override the file, false append to the file
- pcFileName (str) – the full path including filename of file where the information should be written
New in version NX7.5.3.
License requirements: None.
LoadFromLegacynxlibrary¶
-
PhysicalMaterialCollection.
LoadFromLegacynxlibrary
¶ Creates a non-editable material in the part from the legacy (phys_material.
dat) material library definition. The material is identified by the unique material identifier in the phys_material.dat file.
Signature
LoadFromLegacynxlibrary(libraryReference)
Parameters: libraryReference (str) – the unique library reference for a material in this Library Returns: the loaded material Return type: NXOpen.PhysicalMaterial
New in version NX7.5.0.
License requirements: None.
LoadFromLibrary¶
-
PhysicalMaterialCollection.
LoadFromLibrary
¶ Creates a non-editable material in the part from a material library name.
Signature
LoadFromLibrary(pcLibName, pcMatlName)
Parameters: - pcLibName (str) – the fully qualified library name or if the leaf it will use the current directory, followed by the user and site directories set up in the customer defaults
- pcMatlName (str) – the material name
Returns: the loaded material
Return type: New in version NX7.5.3.
License requirements: None.
LoadFromMatmlLibrary¶
-
PhysicalMaterialCollection.
LoadFromMatmlLibrary
¶ Creates a non-editable material in the part from a MatML file definition.
The material is identified by the library name and the unique material name. If the library name is not fully qualified, it will attempt to find a MatML library with this name in the current directory, followed by the specified customer defaults values for the user and site MatML libraries. If the customer defaults are using the file format, it will look in the directory where the specified file is located.
Signature
LoadFromMatmlLibrary(libraryName, materialName)
Parameters: - libraryName (str) – the fully qualified library name or if the leaf it will use the current directory, followed by the user and site directories set up in the customer defaults
- materialName (str) – the material name
Returns: the loaded material
Return type: New in version NX6.0.2.
License requirements: None.
LoadFromNxlibrary¶
-
PhysicalMaterialCollection.
LoadFromNxlibrary
¶ Creates a non-editable material in the part from a NX Material Library definition.
It is preferable to use either NX MatML or NX Legacy library versions as they will have better performance.
Signature
LoadFromNxlibrary(libraryReference)
Parameters: libraryReference (str) – the unique library reference for a material in this Library Returns: the loaded material Return type: NXOpen.PhysicalMaterial
New in version NX6.0.0.
License requirements: None.
LoadFromNxmatmllibrary¶
-
PhysicalMaterialCollection.
LoadFromNxmatmllibrary
¶ Creates a non-editable material in the part from a NX MatML material definition.
Signature
LoadFromNxmatmllibrary(materialName)
Parameters: materialName (str) – the unique material name from within this Library Returns: the loaded material Return type: NXOpen.PhysicalMaterial
New in version NX7.5.0.
License requirements: None.
LoadMaterialItemRevision¶
-
PhysicalMaterialCollection.
LoadMaterialItemRevision
¶ Creates a non-editable material in the part from a Teamcenter material item revision.
Signature
LoadMaterialItemRevision(pcMatlItem, pcRevisionID)
Parameters: - pcMatlItem (str) – the material item
- pcRevisionID (str) – the revision identifier
Returns: the loaded material
Return type: New in version NX7.5.3.
License requirements: None.
OutputMaterialsToLibrary¶
-
PhysicalMaterialCollection.
OutputMaterialsToLibrary
¶ Writes out materials to a material library file.
These materials can be local material definitions or material definitions from other material libraries. The combination of the material name and library name identify a material definition. If the material definition is for a local material, the name is specified and the library name is specified as “”. Write access is needed for the Exported library.
Signature
OutputMaterialsToLibrary(pcMatlNames, pcLibNames, pcExportedLibName)
Parameters: - pcMatlNames (list of str) – Array of identifiers of the materials to be exported
- pcLibNames (list of str) – Array of library names corresponding to the material names
- pcExportedLibName (str) – The library to write the material definitions to
New in version NX6.0.2.
License requirements: None.
UpdateMaterialsInLibrary¶
-
PhysicalMaterialCollection.
UpdateMaterialsInLibrary
¶ Updates the materials in a material library file.
Write access is needed for this operation.
Signature
UpdateMaterialsInLibrary(tEditedMatl, pMatlNames, pcLibName)
Parameters: - tEditedMatl (list of
NXOpen.PhysicalMaterial
) – Array of loaded material tags - pMatlNames (list of str) – Array of the material names which match the name in the library that should take the properties of the corresponding material (tEditedMatl)
- pcLibName (str) – Library to modify
New in version NX6.0.2.
License requirements: None.
- tEditedMatl (list of