ModelingViewHighQualityImageShadeMethod Enumeration¶
NXOpen.ModelingViewHighQualityImage.ShadeMethod is an alias for NXOpen.ModelingViewHighQualityImageShadeMethod
-
class
NXOpen.
ModelingViewHighQualityImageShadeMethod
¶ Bases:
object
Describes the method to be used to generate a High Quality Image
Enum Members
- is assigned a uniform color. “
- “Gouraud”, ” Provides smooth interpolated colors.
- Not quite as fast as Flat shading. “
- “Phong”, ” Provides smoother highlights than Gouraud shading,
- but otherwise supports the same level of functionality. “
- “Improved”, ” Shading with textures material parameters highlights and shadows.
- imilar quality to photo-realistic but significantly faster. “
- “Preview”, ” An improvement over the Improved method. Preview adds
support for transparency without the requirement to also anti-alias the image. “
“PhotoRealistic”, ” All the features of the Improved method, plus support foranti-aliasing and transparency. Images shaded with this mode could take two to three times longer to render than those using the Improved method. “
“RayTraced”, ” Produces photo-realistic images generated with ray tracing.This method is slower than photo-realistic, but it correctly anti-aliases, or renders, textures. “
“RayTracedFfa”, ” Same as the Ray Traced option, but with- Feature Following Anti-aliasing. “
- “Radiosity”, ” An iterative light processing method where indirect lighting
in a scene is derived from direct light bouncing off of surfaces before an image is rendered. Use this method when physically accurate lighting is required for your modeled scene. “
“HybridRadiosity”, ” Uses standard rendering techniques to calculate direct lightingtogether with radiosity processing for indirect lighting for image rendering. Use this method over Radiosity when precise direct lighting effects are also required.”
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.