HumanDataReferencePointType Enumeration¶
NXOpen.HumanData.ReferencePointType is an alias for NXOpen.HumanDataReferencePointType
-
class
NXOpen.
HumanDataReferencePointType
¶ Bases:
object
This enum represents the location of the reference point
Enum Members
Enum Member Enum Member Description No Indicate no reference pointLeftEye Indicate reference point at the left eyeRightEye Indicate reference point at the right eyeHPoint Indicate reference point at the H-pointLeftToe Indicate reference point at the left toeRightToe Indicate reference point at the right toeNumberReferences Indicate the number of reference point types-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-