HumanDataSegmentScalingType Enumeration¶
NXOpen.HumanData.SegmentScalingType is an alias for NXOpen.HumanDataSegmentScalingType
-
class
NXOpen.
HumanDataSegmentScalingType
¶ Bases:
object
This enum represents the types of the segment scaling variable names
Enum Members
Enum Member Enum Member Description Head Indicate scaling of headNeck Indicate scaling of neckTorso Indicate scaling of torsoUpperArm Indicate scaling of upper_armLowerArm Indicate scaling of lower_armHand Indicate scaling of handLowerTorso Indicate scaling of lower_torsoUpperLeg Indicate scaling of upper_legLowerLeg Indicate scaling of lower_legFoot Indicate scaling of foot-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-