SectionCollectionLoopOption Enumeration¶
NXOpen.SectionCollection.LoopOption is an alias for NXOpen.SectionCollectionLoopOption
-
class
NXOpen.
SectionCollectionLoopOption
¶ Bases:
object
Defines how section are created in
SectionCollection.CreateSectionsUsingCurves()
Enum Members
.
- . csv-table::
header: “Enum Member”, “Enum Member Description” “Separate”, ” One section is created for each loop ” “SeparateOuter”, ” One section per outer loop and enclosed inner loops “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.