ViewShowOrHideType Enumeration

NXOpen.View.ShowOrHideType is an alias for NXOpen.ViewShowOrHideType

class NXOpen.ViewShowOrHideType

Bases: object

Specifies whether a show or hide operation, or both, has just been done

Enum Members

Enum Member Enum Member Description
ShowOnly
HideOnly
BothShowAndHide
InvertShownAndHidden
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.