CurveChainRule Class¶
-
class
NXOpen.
CurveChainRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects end-to-end connected curves from the seed curve.New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the curve chain rule: NXOpen.CurveChainRule |
Method Detail¶
Dispose¶
-
CurveChainRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX9.0.0.
License requirements: None.
GetData¶
-
CurveChainRule.
GetData
¶ Gets the data for the curve chain rule:
NXOpen.CurveChainRule
Signature
GetData()
Returns: a tuple Return type: A tuple consisting of (seedCurve, endCurve, fromSeedStart, gapTolerance). seedCurve is a
NXOpen.Curve
. Seed curve endCurve is aNXOpen.Curve
. End Curve. It can be null (Nothing)fromSeedStart is a bool. True: the chain starts from the start point of the seed curve gapTolerance is a float. Gap tolerance .. versionadded:: NX9.0.0License requirements: None.