FileNewApplication Enumeration¶
-
class
NXOpen.
FileNewApplication
¶ Bases:
object
The application type of the new file being created through a template
Deprecated since version NX9.0.0: Use
NXOpen.FileNew.GetApplicationNames()
that returns all application names.Enum Members
Enum Member Enum Member Description Drafting Specifies a drafting file new templateModeling Specifies a modeling file new templateStudio Specifies a shape studio file new templateAssemblies Specifies an assemblies file new templateGateway Specifies a file new template that leaves the new part in GatewayRoutingElectrical Specifies an electrical routing file new templateRoutingMechanical Specifies a mechanical routing file new templateRoutingLogical Specifies a logical routing file new templateNxsheetmetal Specifies a NX sheet metal file new templateSheetTemplate Specifies a drawing sheet template for Insert Sheet dialogCaeFem Specifies a cae fem file new templateCaeSim Specifies a cae sim file new templateAeroSheetmetal Specifies an Aerospace sheet metal templateFlexPcdSheetmetal Specifies a Flex Printed Circuit Design sheet metal templateCaeAssyFem Specifies a cae assembly fem file new templateCam Specifies a Manufacturing file new templateInspection Specifies a CMM Inspection file new templateMechatronics Specifies a Mechatronics Concept Designer file new templateShipContainer Specifies an NX Ship Container file new templateShipDetail Specifies an NX Ship Detail file new templateShipReference Specifies an NX Ship Reference file new templateShipSystem Specifies an NX Ship System file new templateWelding Specifies an NX Structure Welding Design Control Element templateWeldingJoint Specifies an NX Structure Welding Design Feature templateNxle Specifies an NXLE templateLast Specifies the last application type. New application types should be inserted before this one-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-