SketchPasteBuilder Class¶
-
class
NXOpen.
SketchPasteBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.SketchPasteBuilder
To create a new instance of this class, use
NXOpen.SketchCollection.CreateSketchPasteBuilder()
Default values.
Property Value MoveObject.Associative false MoveObject.CreateTraceLines false MoveObject.Divisions 1 MoveObject.LayerOption Original MoveObject.MoveObjectResult MoveOriginal MoveObject.MoveParents true MoveObject.NumberOfCopies 1 MoveObject.TransformMotion.DeltaEnum ReferenceWcsWorkPart MoveObject.TransformMotion.DeltaXc.Value 0.0 MoveObject.TransformMotion.DeltaYc.Value 0.0 MoveObject.TransformMotion.DeltaZc.Value 0.0 MoveObject.TransformMotion.Option Dynamic New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
InitialPasteLocation | Returns or sets the initial paste location, this is mainly used to define default paste location of sketch objects |
MoveObject | Returns the move object |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ResetInitialPasteLocation | Reset the initial paste location, after this previously set initial paste location will not be used |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
InitialPasteLocation¶
-
SketchPasteBuilder.
InitialPasteLocation
¶ Returns or sets the initial paste location, this is mainly used to define default paste location of sketch objects
-------------------------------------
Getter Method
Signature
InitialPasteLocation()
Returns: Drop location coordinates in absolute Return type: NXOpen.Point3d
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InitialPasteLocation(dropLocation)
Parameters: dropLocation ( NXOpen.Point3d
) – Drop location coordinates in absoluteNew in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
MoveObject¶
-
SketchPasteBuilder.
MoveObject
¶ Returns the move object
-------------------------------------
Getter Method
Signature
MoveObject()
Returns: Return type: NXOpen.Features.MoveObjectBuilder
New in version NX7.5.0.
License requirements: None.
Method Detail¶
ResetInitialPasteLocation¶
-
SketchPasteBuilder.
ResetInitialPasteLocation
¶ Reset the initial paste location, after this previously set initial paste location will not be used
Signature
ResetInitialPasteLocation()
New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
Validate¶
-
SketchPasteBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.