MoveObjectBuilder Class¶
-
class
NXOpen.Features.
MoveObjectBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.MoveObjectBuilder
.Inputs to this class can be convergent objects. To create a new instance of this class, use
NXOpen.Features.BaseFeatureCollection.CreateMoveObjectBuilder()
Default values.
Property Value Associative false CreateTraceLines false Divisions 1 LayerOption Original MoveObjectResult MoveOriginal MoveParents true NumberOfCopies 1 TransformMotion.DeltaEnum ReferenceWcsWorkPart TransformMotion.DeltaXc.Value 0.0 TransformMotion.DeltaYc.Value 0.0 TransformMotion.DeltaZc.Value 0.0 TransformMotion.Option Dynamic New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Associative | Returns or sets the associative flag. |
CreateTraceLines | Returns or sets the create trace lines flag |
Divisions | Returns or sets the distance or angle divisions |
Layer | Returns or sets the layer |
LayerOption | Returns or sets the layer option |
MoveObjectResult | Returns or sets the move rotate result |
MoveParents | Returns or sets the move parents flag. |
NumberOfCopies | Returns or sets the number of copies |
ObjectToMoveObject | Returns the objects to move-rotate |
Tag | Returns the Tag for this object. |
TransformMotion | Returns the transform |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MoveObjectBuilderLayerOptionType Enumeration | Indicates the layer on which moved or copied objects will be placed |
MoveObjectBuilderMoveObjectResultOptions Enumeration | Indicates whether to move or copy objects |
Property Detail¶
Associative¶
-
MoveObjectBuilder.
Associative
¶ Returns or sets the associative flag.
A Move Object feature is created only when Move Parents flag is false.
-------------------------------------
Getter Method
Signature
Associative()
Returns: Return type: bool New in version NX6.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative(associative)
Parameters: associative (bool) – New in version NX6.0.2.
License requirements: None.
CreateTraceLines¶
-
MoveObjectBuilder.
CreateTraceLines
¶ Returns or sets the create trace lines flag
-------------------------------------
Getter Method
Signature
CreateTraceLines()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateTraceLines(createTraceLines)
Parameters: createTraceLines (bool) – New in version NX6.0.0.
License requirements: None.
Divisions¶
-
MoveObjectBuilder.
Divisions
¶ Returns or sets the distance or angle divisions
-------------------------------------
Getter Method
Signature
Divisions()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Divisions(distanceOrAngleDivisions)
Parameters: distanceOrAngleDivisions (int) – New in version NX6.0.0.
License requirements: None.
Layer¶
-
MoveObjectBuilder.
Layer
¶ Returns or sets the layer
-------------------------------------
Getter Method
Signature
Layer()
Returns: Return type: int New in version NX6.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Layer(layer)
Parameters: layer (int) – New in version NX6.0.2.
License requirements: None.
LayerOption¶
-
MoveObjectBuilder.
LayerOption
¶ Returns or sets the layer option
-------------------------------------
Getter Method
Signature
LayerOption()
Returns: Return type: NXOpen.Features.MoveObjectBuilderLayerOptionType
New in version NX6.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
LayerOption(layerOptionType)
Parameters: layerOptionType ( NXOpen.Features.MoveObjectBuilderLayerOptionType
) –New in version NX6.0.2.
License requirements: None.
MoveObjectResult¶
-
MoveObjectBuilder.
MoveObjectResult
¶ Returns or sets the move rotate result
-------------------------------------
Getter Method
Signature
MoveObjectResult()
Returns: Return type: NXOpen.Features.MoveObjectBuilderMoveObjectResultOptions
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MoveObjectResult(moveObjectResult)
Parameters: moveObjectResult ( NXOpen.Features.MoveObjectBuilderMoveObjectResultOptions
) –New in version NX6.0.0.
License requirements: None.
MoveParents¶
-
MoveObjectBuilder.
MoveParents
¶ Returns or sets the move parents flag.
The parents of selected objects will be moved only when Associative flag is false.
-------------------------------------
Getter Method
Signature
MoveParents()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MoveParents(moveParents)
Parameters: moveParents (bool) – New in version NX6.0.0.
License requirements: None.
NumberOfCopies¶
-
MoveObjectBuilder.
NumberOfCopies
¶ Returns or sets the number of copies
-------------------------------------
Getter Method
Signature
NumberOfCopies()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfCopies(numCopies)
Parameters: numCopies (int) – New in version NX6.0.0.
License requirements: None.
ObjectToMoveObject¶
-
MoveObjectBuilder.
ObjectToMoveObject
¶ Returns the objects to move-rotate
-------------------------------------
Getter Method
Signature
ObjectToMoveObject()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX6.0.0.
License requirements: None.
TransformMotion¶
-
MoveObjectBuilder.
TransformMotion
¶ Returns the transform
-------------------------------------
Getter Method
Signature
TransformMotion()
Returns: Return type: NXOpen.GeometricUtilities.ModlMotion
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
MoveObjectBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.