MoveObjectBuilderLayerOptionType Enumeration

NXOpen.Features.MoveObjectBuilder.LayerOptionType is an alias for NXOpen.Features.MoveObjectBuilderLayerOptionType

class NXOpen.Features.MoveObjectBuilderLayerOptionType

Bases: object

Indicates the layer on which moved or copied objects will be placed

Enum Members

Enum Member Enum Member Description
Original
Original Layer
Work
Work Layer
AsSpecified
As Specified Layer
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.