FaceConnectedBlendRule Class¶
-
class
NXOpen.
FaceConnectedBlendRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects all connected blend faces.New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the Connected Blend Faces rule: NXOpen.FaceConnectedBlendRule @return Seed face which creates this rule |
GetDefiningData | Gets the data for the Connected Blend Faces rule: NXOpen.FaceConnectedBlendRule |
Method Detail¶
Dispose¶
-
FaceConnectedBlendRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX5.0.0.
License requirements: None.
GetData¶
-
FaceConnectedBlendRule.
GetData
¶ Gets the data for the Connected Blend Faces rule:
NXOpen.FaceConnectedBlendRule
Signature
GetData()
Returns: Seed face which creates this rule Return type: NXOpen.Face
New in version NX5.0.0.
License requirements: None.
GetDefiningData¶
-
FaceConnectedBlendRule.
GetDefiningData
¶ Gets the data for the Connected Blend Faces rule:
NXOpen.FaceConnectedBlendRule
Signature
GetDefiningData()
Returns: a tuple Return type: A tuple consisting of (seedFace, includeBlendLike, includeUnlabeledBlend, feature). seedFace is a
NXOpen.Face
. Seed face which creates this rule includeBlendLike is a bool. true if the rule is to identify any blend-like faces includeUnlabeledBlend is a bool. true if the rule is to include unlabeled blend faces feature is aNXOpen.Features.Feature
. Feature which creates this rule .. versionadded:: NX8.5.0License requirements: None.