SketchStatus Enumeration¶
NXOpen.Sketch.Status is an alias for NXOpen.SketchStatus
-
class
NXOpen.
SketchStatus
¶ Bases:
object
Represents the status of the sketch
Enum Members
Enum Member Enum Member Description Unknown NotEvaluated UnderConstrained More constraints are needed to fully constrain the sketchWellConstrained The sketch is fully constrainedOverConstrained The sketch has more constraints than is neededInconsistentlyConstrained The sketch has conflicting constraints-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-