MeasurePolarArea Class¶
-
class
NXOpen.
MeasurePolarArea
¶ Bases:
NXOpen.SingleMeasure
Represents a single valued polar area measurement
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
MeasurementType | Returns the type of the measurement |
Value | Returns the value of the measurement |
Methods¶
Method | Description |
---|---|
CreateEmbeddedObject | Creates an embedded measurement. |
CreateFeature | Creates and returns a measurement feature @return |
Dispose | Free resources associated with the measure. |
Information | Display information about a measurement. |
Method Detail¶
CreateEmbeddedObject¶
-
MeasurePolarArea.
CreateEmbeddedObject
¶ Creates an embedded measurement.
The name of the measurement can be used in an expression formula.
Signature
CreateEmbeddedObject()
Returns: a tuple Return type: A tuple consisting of (measurement, name). measurement is a NXOpen.Scalar
. the measurement name is a str. the name of the measurementNew in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CreateFeature¶
-
MeasurePolarArea.
CreateFeature
¶ Creates and returns a measurement feature
Signature
CreateFeature()
Returns: Return type: NXOpen.Measure
New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)