GenericMeasure Class¶
-
class
NXOpen.
GenericMeasure
¶ Bases:
NXOpen.TransientObject
Represents a single valued measurement
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
MeasurementType | Returns the type of the measurement |
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the measure. |
Information | Display information about a measurement. |
Enumerations¶
GenericMeasureType Enumeration | The types for a measurement |
Property Detail¶
MeasurementType¶
-
GenericMeasure.
MeasurementType
¶ Returns the type of the measurement
-------------------------------------
Getter Method
Signature
MeasurementType()
Returns: Return type: NXOpen.GenericMeasureType
New in version NX4.0.0.
License requirements: None.
Method Detail¶
Dispose¶
-
GenericMeasure.
Dispose
¶ Free resources associated with the measure.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX4.0.0.
License requirements: None.