SketchPatternType Enumeration¶
NXOpen.SketchPattern.Type is an alias for NXOpen.SketchPatternType
-
class
NXOpen.
SketchPatternType
¶ Bases:
object
Represents the pattern type of the constraint
Enum Members
Enum Member Enum Member Description Linear The pattern type is linear patternCircular The pattern type is circular patternMirror The pattern type is mirror pattern-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-