NXObjectDateAndTimeFormat Enumeration

NXOpen.NXObject.DateAndTimeFormat is an alias for NXOpen.NXObjectDateAndTimeFormat

class NXOpen.NXObjectDateAndTimeFormat

Bases: object

Specifies the format of the date and time attribute.

Enum Members

Enum Member Enum Member Description
Numeric
2004/04/28 22:06:15
Textual
28-Apr-2004 22:06:15
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.