SketchAlongPathBuilderSketchOrientationType Enumeration¶
NXOpen.SketchAlongPathBuilder.SketchOrientationType is an alias for NXOpen.SketchAlongPathBuilderSketchOrientationType
-
class
NXOpen.
SketchAlongPathBuilderSketchOrientationType
¶ Bases:
object
Indicates the sketch orientation method.
For the sketch orientation type is ‘Automatic’: two set of * datum axes are created if the path contains a shared edge, one set of each face. For laminar edge * one set of datum axes is created. If the path contains only wireframe the two set of axes are created. * For the sketch orientation type is ‘Relative to face’: one set of datum axes is craeted using the orienting faces * For the sketch orientation type is ‘Use curve parameter’: one set of datum axes is created using the the curve parameter
Enum Members
Enum Member Enum Member Description Automatic AutomaticRelativeToFace Relative to faceUseCurveParameters Based on curve parameter-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-