ViewRenderingStyleType Enumeration

NXOpen.View.RenderingStyleType is an alias for NXOpen.ViewRenderingStyleType

class NXOpen.ViewRenderingStyleType

Bases: object

Describes the rendering style for geometry displayed in the view.

Enum Members

Enum Member Enum Member Description
ShadedWithEdges  
ShadedWithBodyColorEdges  
Shaded  
WireframeWithDimEdges  
WireframeWithHiddenEdges  
WireframeWithDashedEdges  
Studio  
FaceAnalysis  
PartiallyShaded  
StaticWireframe  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.