MeasureBodies Class¶
-
class
NXOpen.
MeasureBodies
¶ Bases:
NXOpen.GenericMeasure
Represents the measurement specific mass properties for a set of bodies
To create or edit an instance of this class, use
NXOpen.MeasureFaceBuilder
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Area | Returns the value for area of the measurement |
Centroid | Returns the centroid point of the measurement |
InformationUnit | Returns or sets the family of units for mass properties in the information window |
Mass | Returns the value for mass of the measurement |
MeasurementType | Returns the type of the measurement |
RadiusOfGyration | Returns the value for radius of gyration of the measurement |
Volume | Returns the value for volume of the measurement |
Weight | Returns the value for weight of the measurement |
Methods¶
Method | Description |
---|---|
CreateEmbedded | Creates and returns an embedded measurement expression. |
CreateEmbeddedObject | Creates an embedded measurement. |
CreateFeature | Creates and returns a measurement feature to obtain mass properties of solid bodies @return |
Dispose | Free resources associated with the measure. |
Information | Display information about a measurement. |
Enumerations¶
MeasureBodiesActiveValue Enumeration | Indicates the type of embedded measurement to create |
MeasureBodiesAnalysisUnit Enumeration | Indicates the family of units used in mass property information listings |
Property Detail¶
Area¶
-
MeasureBodies.
Area
¶ Returns the value for area of the measurement
-------------------------------------
Getter Method
Signature
Area()
Returns: Return type: float New in version NX4.0.0.
License requirements: None.
Centroid¶
-
MeasureBodies.
Centroid
¶ Returns the centroid point of the measurement
-------------------------------------
Getter Method
Signature
Centroid()
Returns: Return type: NXOpen.Point3d
New in version NX4.0.0.
License requirements: None.
InformationUnit¶
-
MeasureBodies.
InformationUnit
¶ Returns or sets the family of units for mass properties in the information window
-------------------------------------
Getter Method
Signature
InformationUnit()
Returns: Return type: NXOpen.MeasureBodiesAnalysisUnit
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InformationUnit(unitValue)
Parameters: unitValue ( NXOpen.MeasureBodiesAnalysisUnit
) –New in version NX4.0.0.
License requirements: None.
Mass¶
-
MeasureBodies.
Mass
¶ Returns the value for mass of the measurement
-------------------------------------
Getter Method
Signature
Mass()
Returns: Return type: float New in version NX4.0.0.
License requirements: None.
RadiusOfGyration¶
-
MeasureBodies.
RadiusOfGyration
¶ Returns the value for radius of gyration of the measurement
-------------------------------------
Getter Method
Signature
RadiusOfGyration()
Returns: Return type: float New in version NX4.0.0.
License requirements: None.
Method Detail¶
CreateEmbedded¶
-
MeasureBodies.
CreateEmbedded
¶ Creates and returns an embedded measurement expression.
Deprecated: Use CreateEmbeddedObject instead
Signature
CreateEmbedded(measurementType)
Parameters: measurementType ( NXOpen.MeasureBodiesActiveValue
) –Returns: Return type: str New in version NX4.0.0.
Deprecated since version NX5.0.1: Use
NXOpen.MeasureBodies.CreateEmbeddedObject()
instead.License requirements: solid_modeling (“SOLIDS MODELING”)
CreateEmbeddedObject¶
-
MeasureBodies.
CreateEmbeddedObject
¶ Creates an embedded measurement.
The name of the measurement can be used in an expression formula.
Signature
CreateEmbeddedObject(measurementType)
Parameters: measurementType ( NXOpen.MeasureBodiesActiveValue
) –Returns: a tuple Return type: A tuple consisting of (measurement, name). measurement is a NXOpen.Scalar
. the measurement name is a str. the name of the measurementNew in version NX5.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
CreateFeature¶
-
MeasureBodies.
CreateFeature
¶ Creates and returns a measurement feature to obtain mass properties of solid bodies
Signature
CreateFeature()
Returns: Return type: NXOpen.Measure
New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)