NXObjectAttributeInformation_Struct Struct¶
NXOpen.NXObject.AttributeInformation is an alias for NXOpen.NXObjectAttributeInformation_Struct
-
class
NXOpen.
NXObjectAttributeInformation_Struct
¶ Bases:
object
Contains attribute information.
All the data members of this struct are updated with values from the attribute (some possibly to None) when an attribute is read.
The following data members of this struct are not used (they are ignored) when setting an attribute: Alias Inherited Override Required Unset Locked OwnedBySystem PdmBased
The following data of an attribute cannot be edited once the attribute is set: Type Title TitleAlias Array ArrayElementIndex The dimensionality of the Unit specification (cannot change from mm to microA, but from mm to cm is fine)
The following data of an attribute can be set and modified if and only if the attribute is not associated with a template: Category
The following data of an attribute can be set if and only if the attribute is not associated with a template. It cannot be modified once set. Array . Constructor: NXOpen.NXObject.AttributeInformation()
Fields¶
Field | Description |
---|---|
Type | Attribute type |
Category | Attribute category (may be None) |
Title | Attribute title (for arrays, this is the array title without an appended index) |
TitleAlias | Attribute title alias (may be None) (for arrays, this is the array title alias, without an appended index) |
BooleanValue | Boolean (logical) attribute value (the default value is returned when reading templates of non-set attributes) |
IntegerValue | Integer attribute value (the default value is returned when reading templates of non-set attributes) |
RealValue | Real attribute value (the default value is returned when reading templates of non-set attributes) If the attribute has units, it is returned in the display units of the attribute |
StringValue | String attribute value (the default value is returned when reading templates of non-set attributes). |
TimeValue | Time/Date attribute value (the default value is returned when reading templates of non-set attributes). |
CompTimeValue | Time/Date attribute value (the default value is returned when reading templates of non-set attributes). |
ReferenceValue | Reference string of a string type attribute (it is None if it is a ‘normal’ string attribute). |
Inherited | The attribute is inherited from another object and not overridden |
IsOverride | The attribute is overriding an inherited attribute |
Locked | The attribute is locked. |
OwnedBySystem | This attribute is a reserved system attribute. |
Required | The attribute is required on the given object |
Unset | The attribute has not been set (i. |
Array | The attribute is an array attribute |
PdmBased | The attribute is PDM-based |
NotSaved | The attribute is transient - it will not be saved on part save |
ArrayElementIndex | If this struct represents an array attribute element, this is the index (numerical, starting with 0). |
Unit | The display units, if any, if the attribute is a real-type attribute |
Expression | The expresssion referenced by the attribute (only supported if the referenceValue is None) |
Type¶
-
NXObjectAttributeInformation_Struct.
Type
¶ Attribute type
-------------------------------------
Field Value Type:
NXOpen.NXObjectAttributeType
Category¶
-
NXObjectAttributeInformation_Struct.
Category
¶ Attribute category (may be None)
-------------------------------------
Field Value Type:str
Title¶
-
NXObjectAttributeInformation_Struct.
Title
¶ Attribute title (for arrays, this is the array title without an appended index)
-------------------------------------
Field Value Type:str
TitleAlias¶
-
NXObjectAttributeInformation_Struct.
TitleAlias
¶ Attribute title alias (may be None) (for arrays, this is the array title alias, without an appended index)
-------------------------------------
Field Value Type:str
BooleanValue¶
-
NXObjectAttributeInformation_Struct.
BooleanValue
¶ Boolean (logical) attribute value (the default value is returned when reading templates of non-set attributes)
-------------------------------------
Field Value Type:bool
IntegerValue¶
-
NXObjectAttributeInformation_Struct.
IntegerValue
¶ Integer attribute value (the default value is returned when reading templates of non-set attributes)
-------------------------------------
Field Value Type:int
RealValue¶
-
NXObjectAttributeInformation_Struct.
RealValue
¶ Real attribute value (the default value is returned when reading templates of non-set attributes) If the attribute has units, it is returned in the display units of the attribute
-------------------------------------
Field Value Type:float
StringValue¶
-
NXObjectAttributeInformation_Struct.
StringValue
¶ String attribute value (the default value is returned when reading templates of non-set attributes).
-------------------------------------
Field Value Type:str
TimeValue¶
-
NXObjectAttributeInformation_Struct.
TimeValue
¶ Time/Date attribute value (the default value is returned when reading templates of non-set attributes).
See
NXOpen.NXObjectDateAndTimeFormat
for valid formats. The time value held here is in the current time zone of the machine running the program. NOTE: if both TimeValue and CompTimeValue are unset (None and (0,0), respectively) when the attribute is set, then the attribute will be set to current time and date.-------------------------------------
Field Value Type:str
CompTimeValue¶
-
NXObjectAttributeInformation_Struct.
CompTimeValue
¶ Time/Date attribute value (the default value is returned when reading templates of non-set attributes).
The time value held here is in the current time zone of the machine running the program.
-------------------------------------
Field Value Type:
NXOpen.NXObjectComputationalTime_Struct
ReferenceValue¶
-
NXObjectAttributeInformation_Struct.
ReferenceValue
¶ Reference string of a string type attribute (it is None if it is a ‘normal’ string attribute).
Only supported if the expression reference is None.
-------------------------------------
Field Value Type:str
Inherited¶
-
NXObjectAttributeInformation_Struct.
Inherited
¶ The attribute is inherited from another object and not overridden
-------------------------------------
Field Value Type:bool
IsOverride¶
-
NXObjectAttributeInformation_Struct.
IsOverride
¶ The attribute is overriding an inherited attribute
-------------------------------------
Field Value Type:bool
Locked¶
-
NXObjectAttributeInformation_Struct.
Locked
¶ The attribute is locked.
When an existing attribute is read, this flag indicates that the attribute cannot currently be modified. The flag is set if the attribute is created from a template that has the ‘Locked’ flag, or if it is reserved by the system or by some other mechanism. When an unset attribute template is read, this flag indicates whether attributes created from the template will be locked when the part is saved and reloaded.
-------------------------------------
Field Value Type:bool
OwnedBySystem¶
-
NXObjectAttributeInformation_Struct.
OwnedBySystem
¶ This attribute is a reserved system attribute.
When this flag is set, the attribute can be set and removed only by the system. It is also created locked. It cannot be unlocked.
-------------------------------------
Field Value Type:bool
Required¶
-
NXObjectAttributeInformation_Struct.
Required
¶ The attribute is required on the given object
-------------------------------------
Field Value Type:bool
Unset¶
-
NXObjectAttributeInformation_Struct.
Unset
¶ The attribute has not been set (i.
e. has no value) on the object (used when getting attribute information)
-------------------------------------
Field Value Type:bool
Array¶
-
NXObjectAttributeInformation_Struct.
Array
¶ The attribute is an array attribute
-------------------------------------
Field Value Type:bool
PdmBased¶
-
NXObjectAttributeInformation_Struct.
PdmBased
¶ The attribute is PDM-based
-------------------------------------
Field Value Type:bool
NotSaved¶
-
NXObjectAttributeInformation_Struct.
NotSaved
¶ The attribute is transient - it will not be saved on part save
-------------------------------------
Field Value Type:bool
ArrayElementIndex¶
-
NXObjectAttributeInformation_Struct.
ArrayElementIndex
¶ If this struct represents an array attribute element, this is the index (numerical, starting with 0).
After reading an attribute, it is valid only if ‘Unset’ is ‘false’ and ‘Array’ is ‘true’. The array size can be resized only one element at a time (adding or removing the last element).
-------------------------------------
Field Value Type:int
Unit¶
-
NXObjectAttributeInformation_Struct.
Unit
¶ The display units, if any, if the attribute is a real-type attribute
-------------------------------------
Field Value Type:
NXOpen.Unit
Expression¶
-
NXObjectAttributeInformation_Struct.
Expression
¶ The expresssion referenced by the attribute (only supported if the referenceValue is None)
-------------------------------------
Field Value Type:
NXOpen.Expression