LoadOptionsManagedModeLoadMethod Enumeration¶
NXOpen.LoadOptions.ManagedModeLoadMethod is an alias for NXOpen.LoadOptionsManagedModeLoadMethod
-
class
NXOpen.
LoadOptionsManagedModeLoadMethod
¶ Bases:
object
Options for specifying how to configure assembly structure in managed mode
Enum Members
Enum Member Enum Member Description ByRevisionRule use the assembly structure configured by revision rule for loadAsSaved use assembly structure in the part file for load-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-