PartCollectionRefsetOption Enumeration¶
NXOpen.PartCollection.RefsetOption is an alias for NXOpen.PartCollectionRefsetOption
-
class
NXOpen.
PartCollectionRefsetOption
¶ Bases:
object
Controls the reference set used when setting the work component.
See
NXOpen.PartCollection.SetWorkComponent()
Enum Members
- and restore the reference set of the previous work component “
- “Current”, ” Use the component’s current reference set,
- and restore the reference set of the previous work component “
- “PreserveRefset”, ” Use the component’s current reference set,
and do not reset the reference set of the previous work component “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.